SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
The PCIe Subsystem has different requirements based upon whether it is operated in Root Port (RP) or End Point (EP) mode. The PCIe subsystem does not have DMA capabilities built into it. It has internal slave and master ports connected to the device-level interconnect.
An external DMA engine can make burst data read/writes on the slave port and the master port on PCIe subsystem can initiate reads/writes to memory on behalf of a remote PCIe device.
The PCIe subsystem does not specify the DMA protocol that is used for data transfers. The software implementations on the two ends of the PCIe link implement a data transfer protocol that is compatible with each other.
As a result, there will be several software drivers required – one driver that will manage the PCIe subsystem in RP mode and another set of drivers that will run on the RP side and will manage each of the End Points connected to the PCIe subsystem RP.
Similarly, when PCIe subsystem is operating as an End Point, there are two drivers – one to manage the PCIe subsystem from the device side and another driver that will run on the device operating as the Root Port.