SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Figure 12-2708 shows how the interrupt mechanism works in the EQEP module.
Eleven interrupt events (PCE, PHE, QDC, WTO, PCU, PCO, PCR, PCM, SEL, IEL, and UTO) can be generated. The interrupt control register (EQEP_QINT_EN_FLG) is used to enable/disable individual interrupt event sources. The interrupt flag register (EQEP_QINT_EN_FLG) indicates if any interrupt event has been latched and contains the global interrupt flag bit (INT). An interrupt pulse is only generated to the interrupt controller if any of the interrupt events is enabled, the flag bit is 1 and the INT flag bit is 0. The interrupt service routine will need to clear the global interrupt flag bit and the serviced event, via the interrupt clear register (EQEP_QINT_CLR_FRC), before any other interrupt pulses are generated. SW can force an interrupt event by way of the interrupt force register (EQEP_QINT_CLR_FRC), which is useful for test purposes.