SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Ordering becomes a concern due to the fact that the VBUSM commands are fragmented and not guaranteed to be returned in order by the VBUSM.C interface. This violates the CBA ordering rules for a single slave endpoint. So the bridge will force read data ordering based on the orderid signal across all masters, as a balance between cost and performance. This means that each read command received from the VBUSM interface with a particular orderid value will have their read data returned in exactly the same order. This means that even if the reads are from different masters, the data will still be returned in order, to reduce the amount of tracking the bridge has to perform. But, if the reads use different orderid values then that read data can be returned in any order, whichever is received first on the VBUSM.C interface.