SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
This register contains the byte count of the transaction error that was captured.
Bits | Field | Type | Reset | Description |
---|---|---|---|---|
31:26 | Reserved | r | 0x0 | Reserved. Read as 0. |
25:16 | cbytecnt | r | 0x0 | Current Byte Count – If this is a timed out transaction, this is the number of bytes that were not returned as of the time the transaction timed out. If this is an unexpected response transaction, then this field is not applicable. |
15:10 | Reserved | r | 0x0 | Reserved. Read as 0. |
9:0 | obytecnt | r | 0x0 | Original Byte Count – If this is a timed out transaction, then this field represents the CBYTECNT value of the original command. If this is an unexpected response transaction, then this field contains the value of the bytecnt of the unexpected transaction (sbytecnt or rbytecnt). |