SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
This module provides proxy buffers for hosts that need to create large data bursts but can only perform small accesses. Examples of this need are for large Message Manager messages, Queue Manager data that is more than a pointer, or DMA Transfer Requests Messages. All of these require larger data sets, from 12 to 128 bytes, and the modules require the entire data on the bus in a single burst. Unfortunately, many CPUs cannot produce bursts to device memory, such as hardware registers, and the largest CPU access is typically 8 bytes. So the proxy provides the ability to access the module with a single burst, and at the same time allows the CPU to access the same data in smaller accesses. The proxy itself does not contain the resources, but it stays in front of other module (target module) that does contain the resources. The proxy will access the target module with the entire data in a single burst, once the host has completed the data.