SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Each EPWM module has one interrupt request line as shown in Figure 12-2644. Mapping interrupt lines to device host interrupt controllers is device specific and is covered in EPWM Integration.
The event-trigger submodule monitors various event conditions (the left side inputs to event-trigger submodule shown in Figure 12-2645) and can be configured to prescale these events before issuing an Interrupt request. The event-trigger prescaling logic can issue Interrupt requests at:
A more detailed look at how the various register bits interact with the Interrupt is shown in Figure 12-2646.
Figure 12-2646 shows the event-trigger's interrupt generation logic. The interrupt-period (EPWM_ETPS[1-0] INTPRD) bits specify the number of events required to cause an interrupt pulse to be generated. The choices available are:
An interrupt cannot be generated on every fourth or more events.
Which event can cause an interrupt is configured by the interrupt selection (EPWM_ETSEL[2-0] INTSEL) bits. The event can be one of the following:
The number of events that have occurred can be read from the interrupt event counter (EPWM_ETPS[3-2] INTCNT) register bits. That is, when the specified event occurs the EPWM_ETPS[3-2] INTCNT bits are incremented until they reach the value specified by the EPWM_ETPS[1-0] INTPRD bit field. When EPWM_ETPS[3-2] INTCNT = EPWM_ETPS[1-0] INTPRD the counter stops counting and its output is set. The counter is only cleared when an interrupt is sent to the interrupt controller.
When EPWM_ETPS[3-2] INTCNT reaches EPWM_ETPS[1-0] INTPRD, one of the following behaviors will occur:
Writing to the INTPRD bits will automatically clear the counter INTCNT = 0 and the counter output will be reset (so no interrupts are generated). Writing a 1h to the EPWM_ETFRC[0] INT bit will increment the event counter INTCNT. The counter will behave as described above when INTCNT = INTPRD. When INTPRD = 0h, the counter is disabled and hence no events will be detected and the EPWM_ETFRC[0] INT bit is also ignored.