SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
In self test mode, the CCMR5 compare block is checked for faults by applying internally generated series of test patterns. During self test, the core compare disabled signal is deactivated. If a fault on the CCMR5 module gets detected, a self test error is generated.
When self test mode is entered, the CCMR5 module will generate predetermined test patterns to look for any hardware faults inside it. If a fault is detected, then a self test error flag (STE1) is set, a self test error signal is asserted, and the self test is terminated immediately after entering compare mismatch mode. If no fault is found during self test, the self test complete flag (STC1) will be set. The user needs to poll the R5FSS_CCMSR1 status register to find out the self test status. In both cases – self test terminated and self test completed – the CCMR5 will remain in self test mode and will be idle, and therefore the R5FSS_CCMKEYR1 key register will show the self test key until the mode is switched by writing another key to this register. During the self test operation, the compare error signal output is inactive, irrespective of the compare result. When switched out of self test mode, the core compare disabled signal is de-asserted.
There are two types of patterns generated by CCMR5 during self test mode: compare match test, and compare mismatch test. The CCMR5 first generates compare match test patterns followed by compare mismatch test patterns. During self test, each test pattern is applied on CPU output signal ports of the CCMR5’s compare block and clocked for one cycle.
Self test of CPU output compare logic is done with respect to CPU clock. As mentioned, self test error is indicated by the self test error signal. Whether the self test failed during compare match test or compare mismatch test is indicated by the self test error type flag (STET1) in the R5FSS_CCMSR1 status register. When the block’s self test is completed, the corresponding self test complete flag (STC1) is set.
During self test, both CPUs can execute normally, but the compare logic will not be checking any CPU signals. Also, during self test, only the compare unit logic is tested. The self test is not interruptible.