SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
The module outputs events about queue levels that can be used by an external module for statistics or interrupts.
Each queue has
The event number is programmable per queue in the RINGACC_EVENT_j register. This event occurs when the state machine updates the final occupancy for the queue. In ring mode this is when the response from the memory access returns, while in other queue modes this is when the operation is processed.
An event number programmed to 0xFFFF indicates to not produce an event for that ring when an event is not necessary. The register event number fields reset to 0xFFFF, so they must be programmed to a valid value before events will be generated. This applies to the monitor event number fields as well.