SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
In UDMASS_INTR_AGGR0, the INTR_AGGR will provide a set of Global event multicast (UDMA_INTA_MCMAP_j) registers. These registers allow an ingress Global event on its ingress ETL interface to be mapped into two egress Global events on two separate egress ETL interfaces. A set of registers map the ingress Global event index (1-N) into two arbitrary egress event indices.