SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
North Bridges are implemented in the SoC with the parameters shown in Table 10-666 and Table 10-667.
Parameter | Value | Description |
---|---|---|
Number of sources | 2 | The number of VBUSM source interfaces |
Source 0 | CBASS MSMC_SLV0 to MSMC0 | Source 0 |
Source 1 | CBASS MSMC_SLV1 to MSMC0 | Source 1 |
source_oidmap[0] | 0-7 | This defines the orderid mapping to the VBUSM sources. The index represents the source number. The values are integer. |
source_oidmap[1] | 8-15 | |
start64k | 0x0060000000 | This defines the starting address of the memory in VBUSM.C that uses the 64-KB table. |
num64k | 8192 | This defines the number of entries in the 64-KB table. |
Parameter | Value | Description |
---|---|---|
Number of sources | 2 | The number of VBUSM source interfaces |
Source 0 | CBASS MSMC_DDR_0 to MSMC1 | Source 0 |
Source 1 | CBASS MSMC_DDR_1 to MSMC1 | Source 1 |
source_oidmap[0] | 0-7 | This defines the orderid mapping to the VBUSM sources. The index represents the source number. The values are integer. |
source_oidmap[1] | 8-15 | |
start16m[0] | 0x0080000000 | This defines the starting address of the memory in VBUSM.C that uses the 16-MB table. The index is for each of the 16-MB regions. |
start16m[1] | 0x0800000000 | |
num16m[0] | 128 | This defines the number of entries in the 16-MB table. The index is for each 16-MB region. |
num16m[1] | 8192 |