SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
The PSIL events are also routed based on the event number. An event map defines which event number range maps to the destination ETL events of that endpoint. All source events from endpoints will be routed to a destination endpoint based on this event map. When the event number does not map to any endpoint, then it is routed to a default output event interface that connects to an event aggregator to map them to interrupts.
In addition to PSI-L endpoints, event endpoints are supported. These events connect to the same event interconnect as the PSI-L endpoints and pass events in the same way. An event endpoint can be a producer or consumer of events, and the same event mapping can apply to an event or PSI-L endpoint.