SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
In addition to the global reset sources the device can have a number of local reset sources for each power domain. The local reset sources can be cold or warm reset sources. They can be software-controlled or hardware-triggered. Table 3-32 identifies the possible types of hardware-triggered local cold reset sources. Some power domains can support one or both of these local cold reset sources. The table does not list the software-triggered local warm reset sources that are listed in the reset management section of the respective power domains. A local reset source signal received by the reset manager resets only a specific part of the device (for example, some modules/subsystems within the power domain).
| Type(1) | Name | Source/Control | Description |
|---|---|---|---|
| H/C | <Power domain>_RET_RST | PRCM | Asserted only for a power domain state transition from OFF to ON-ACTIVE state |
| H/C | <Power domain>_RST | PRCM | Asserted for any power domain transition from OFF to ON-ACTIVE state |