SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
In the next scheme (see Figure 34-13), it is assumed that the new version of the firmware Flash Loader Host is located in the PC host. In the same way, the application loaded to device internal L3 On-chip RAM (using the peripheral boot function of the device ROM code) is called Flash Loader Second.