SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
If the input is YUV422 and YUV444_MODE or YUVtoRGB_MODE is selected (SRC_FMT [FMT] =3, SRC_FMT [FMT2]=1 or 2), this module up-samples YUV422 to YUV444. (In YUVtoRGB_MODE, the next RGB2RGB module also converts YUV to RGB.) The module refers to SRC_FMT [FMT3] for the chroma sampling position. If the value is 0 (co-sited), the up-sampling is done in the way in Figure 9-65If it is 1, it is done in the way Figure 9-66
Figure 9-65 ISS ISP IPIPE YUV422 to 444 in co-sited mode
Figure 9-66 ISS ISP IPIPE YUV422 to 444 in co-sited mode