SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
When several concurrent channels are latency critical and hardware synchronized, a specific latency cannot be ensured until the target is served. This situation occurs when the number of concurrent channels is greater than the number of available threads.
Four threads are available on the read port, and two threads are available on the write port.
For a hardware-synchronized transfer (memory to peripheral), a minimum bandwidth for a latency-critical transfer must be ensured to avoid collisions between two hardware requests.
Because it is latency critical, the software user is responsible for the following:
The proposed implementation is as follows (see Section 18.1.5.5, Concurrent Software and Hardware Synchronization):
Prevent the regular channel queue from exceeding more than a programmable (3, 2, or 1) number of threads on the read port and no more than one thread on the write port. This number can be set in the global register DMA4_GCR[13:12] .
The thread reservation is programmable for maximum use of thread resources for concurrent, low-priority channel transfer. Programmability can also allow a partial throughput control by limiting in software the number of concurrent outstanding requests that break the pipelining.
Depending on the DMA4_GCR [13:12] value, the following threadID on the read/write ports are allocated for a high-priority channel:
Read port priority thread reservation:
Write port priority thread reservation:
Regardless of whether the enabled channels are high priority, only the setting of the DMA4_GCR[13:12] value forces the thread reservation to these values. Set the appropriate value to avoid losing threads using only regular channels.
To have an independent read and write priority context, a per-channel bit (DMA4_CCRi[26]) is added for write priority, and the previous priority bit becomes read priority bit (DMA4_CCRi[6]).
The device has one priority bit per logical channel, not one priority bit per port.