SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The VIP_PARSER supports a maximum of 8 different Channel IDs per Port. The Channel IDs must be in the range {0:7} (3 bits). In the source multiplex, only one source can be a split line source and have the same Channel ID as one of the non-split line sources.
This scenario involves an external NTSC decoder which supports 8 D1 cameras. The external NTSC decoder will downscale the 8 sources to SIF format. However, one camera source will be sent in the multiplex as both the downscaled version and the original D1 sized version. They will both have the same Channel ID. However, the D1 version will be sent as a split-line. The source multiplex will thus have 9 maximum streams.
The VIP_PARSER (for TI Line Mux Mode only), will left shift the Channel ID by one. Bit 0 is used as an indicator whether the Source is a split-line source or a normal non-split line source. Only one of the nine inputs can be a split line source.
| Channel ID Sent to VPDMA | ||
| Source Input Channel ID | Non-split Line | Split Line |
| 0x0 | 0x0 | 0x1 |
| 0x1 | 0x2 | 0x3 |
| 0x2 | 0x4 | 0x5 |
| 0x3 | 0x6 | 0x7 |
| 0x4 | 0x8 | 0x9 |
| 0x5 | 0xA | 0xB |
| 0x6 | 0xC | 0xD |
| 0x7 | 0xE | 0xF |
All subsequent references to the Camera Source, such as in a VPDMA return descriptor, will reference the remapped Channel ID.
The VIP_OUTPUT_PORT_A_SRC0_SIZE through VIP_OUTPUT_PORT_A_SRC15_SIZE registers for Port A, and VIP_OUTPUT_PORT_B_SRC0_SIZE through VIP_OUTPUT_PORT_B_SRC15_SIZE registers for Port B and the VIP_OUTPUT_PORT_A_SRC_FID and VIP_OUTPUT_PORT_B_SRC_FID status registers reflect the remapped Channel ID when the port is in TI Line Mux mode.