SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
The local power-down mode is requested by setting the DCAN_CTL[24] PDR bit (=1).
The DCAN then finishes all transmit requests of the message objects. When all requests are done, DCAN waits until a bus idle state is recognized. Then it will automatically set the DCAN_CTL[0] INIT bit to prevent any further CAN transfers, and it will also set the DCAN_ES[10] PDA bit. With setting the PDA bit, the DCAN module indicates that the local power-down mode has been entered.
During local power-down mode, the internal clocks of the DCAN module are turned off, but there is a wakeup logic (see Section 26.10.4.4.2, Wakeup From Local Power Down) that can be active, if enabled. Also, the actual contents of the control registers can be read back.
In local low-power mode, the software must not clear the INIT bit while PDR is set. If there are any messages in the message RAM which are configured as transmit messages and the application resets the INIT bit, these messages may get sent.