SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
A write to the LCNTn register within the loop body (of either of the loops) is used to dynamically change the iteration count, including pre-maturely terminating the corresponding level. Such a write to LCNTn instruction must be executed at least 2 instructions before the last (ending) instruction of the corresponding loop (x).
It is also possible to skip inner loop dynamically (per iteration of the outer loop) by simply branching across the inner loop within the outer loop context. It is not necessary to explicitly set the inner loop count to 0/1 (loop inactive values). Similarly, a branch out of the outer loop context is possible without setting the outer loop count to inactive values. This relies on the fact that even if the inner or outer loop count has not been set to an inactive value, a loop rewind des not happen unless the loop end PC (LEAn) is encountered.
These features (dynamically changing the loop iteration count, skipping inner/outer loop via branches) are used by the compiler to implement constructs such as last/continue/break and alike.