SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
Packet Length
Specifies the number of bytes in the entire packet. Offset bytes are not included. The sum of the Buffer_Length fields should equal the Packet_Length. Valid only on SOP.
Start of Packet (SOP) Flag
When set, this flag indicates that the descriptor points to a packet buffer that is the start of a new packet. In the case of a single fragment packet, both the SOP and end of packet (EOP) flags are set. Otherwise, the descriptor pointing to the last packet buffer for the packet has the EOP flag set. This flag is initially cleared by the software application before adding the descriptor to the receive queue. This bit is set by the EMAC on SOP descriptors.
End of Packet (EOP) Flag
When set, this flag indicates that the descriptor points to a packet buffer that is last for a given packet. In the case of a single fragment packet, both the start of packet (SOP) and EOP flags are set. Otherwise, the descriptor pointing to the last packet buffer for the packet has the EOP flag set. This flag is initially cleared by the software application before adding the descriptor to the receive queue. This bit is set by the EMAC on EOP descriptors.
Ownership (OWNER) Flag
When set, this flag indicates that the descriptor is currently owned by the EMAC. This flag is set by the software application before adding the descriptor to the receive descriptor queue. This flag is cleared by the EMAC once it is finished with a given set of descriptors, associated with a received packet. The flag is updated by the EMAC on SOP descriptor only. So when the application identifies that the OWNER flag is cleared on an SOP descriptor, it may assume that all descriptors up to and including the first with the EOP flag set have been released by the EMAC. (Note that in the case of single buffer packets, the same descriptor will have both the SOP and EOP flags set.)
End of Queue (EOQ) Flag
When set, this flag indicates that the descriptor in question was the last descriptor in the receive queue for a given receive channel, and that the corresponding receiver channel has halted. This flag is initially cleared by the software application prior to adding the descriptor to the receive queue. This bit is set by the EMAC when the EMAC identifies that a descriptor is the last for a given packet received (also sets the EOP flag), and there are no more descriptors in the receive list (next descriptor pointer is NULL).The software application can use this bit to detect when the EMAC receiver for the corresponding channel has halted. This is useful when the application appends additional free buffer descriptors to an active receive queue. Note that this flag is valid on EOP descriptors only.
Teardown Complete (TDOWNCMPLT) Flag
This flag is used when a receive queue is being torn down, or aborted, instead of being filled with received data. This would happen under device driver reset or shutdown conditions. The EMAC sets this bit in the descriptor of the first free buffer when the tear down occurs. No additional queue processing is performed.
Pass CRC (PASSCRC) Flag
This flag is set by the EMAC in the SOP buffer descriptor if the received packet includes the 4-byte CRC. This flag should be cleared by the software application before submitting the descriptor to the receive queue.
Long (Jabber) Flag
This flag is set by the EMAC in the SOP buffer descriptor, if the received packet is a jabber frame and was not discarded because the RX_CEF_EN bit was set in the SL_MACCONTROL register. Jabber frames are frames that exceed the RXMAXLEN in length, and have CRC, code, or alignment errors.
Short (Fragment) Flag
This flag is set by the EMAC in the SOP buffer descriptor, if the received packet is only a packet fragment and was not discarded because the RX_CSF_EN bit was set in the SL_MACCONTROL register.
Control Flag
This flag is set by the EMAC in the SOP buffer descriptor, if the received packet is an EMAC control frame and was not discarded because the RX_CMF_EN bit was set in the SL_MACCONTROL register.
Overrun Flag
This flag is set by the EMAC in the SOP buffer descriptor, if the received packet was aborted due to a receive overrun.
Packet Error (PKT_ERR) Flag
Packet Contained Error on Ingress:
00 - no error
01 - CRC error on ingress
10 - Code error on ingress
11 - Align error on ingress
VLAN Encapsulated Packet (RX_VLAN_ENCAP)
Indicates when set that the packet data contains a 32-bit VLAN header word that is included in the packet byte count. This field is set by the port to be the value of the CPSW_CONTROL register RX_VLAN_ENCAP bit.
FROM_PORT
Indicates the port number that the packet was received on (ingress to the switch).