SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
Figure 34-1 is an overview of the initialization process and its steps:
Figure 34-1 Initialization ProcessThe first two steps in the initialization process are hardware-oriented; however, they require an understanding of the process of configuring these system interface pins (balls on the device), which have software-configurable functionality. This configuration is an essential part of the chip configuration and is application-dependent. This chapter discusses these system-interface pins and the associated configuration registers that are vital to the correct initialization of the device.