SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
In master and slave modes, the McSPI drives the data lines when SPIEN[x] is asserted.
Each word is transmitted starting with the most-significant bit (MSB).
This section explains the two cases of data transmission determined by the clock phase (PHA) and the type of data transmission using a start-bit (SBE) called the start-bit mode:
When PHA = 0, the first bit of the SPI word to transmit (on the master or the slave data output pin) is valid one-half cycle of SPICLK after the assertion of SPIEN.
Therefore, the first edge of the SPICLK line is used by the master to sample the first data bit sent by the slave. On the same edge, the first data bit sent by the master is sampled by the slave.
On the next SPICLK edge, the received data bit is shifted into the receive shift register and a new data bit is transmitted on the serial data line.
This process continues for a number of pulses on the SPICLK line defined by the SPI word length programmed in the master device, with data being latched on odd-numbered edges and shifted on even-numbered edges. See Figure 26-76.
Figure 26-76 Full-Duplex Transfer Format With PHA = 0When PHA = 1, the first bit of the SPI word to transmit (on the master or the slave data output pin) is valid on the following SPICLK edge (one-half cycle later). This is the sampling edge for the master and slave. A synchronization delay is added between the activation of SPIEN[x] and the first SPICLK edge.
The received data bit is shifted into the shift register on the third SPICLK edge.
This process continues for a number of pulses on the SPICLK line defined by the SPI word length programmed in the master device, with data being latched on even-numbered edges and shifted on odd-numbered edges.
The minimum synchronization delay is one cycle of SPICLK, if the frequency of SPICLK equals the frequency of SPIm_FCLK (McSPIm functional clock) in master mode. The minimum synchronization delay is one-half cycle of SPICLK, if the frequency of SPICLK is lower than the frequency of SPIm_FCLK in the master and slave modes.
When the MCSPI_CHxCONF[23] SBE bit is set to 1, a start-bit is added before the MSB to indicate whether the next SPI word must be handled as a command or as data.
Figure 26-77 shows an example of a data transfer with an extra start-bit.
Figure 26-77 Extended SPI Transfer With a Start-Bit (SBE = 1)