SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
There are three requirements to program descriptors:
If the total length of a descriptor is not a multiple of the block size, data transfer with the ADMA engine may not have been terminated. In this case, the controller returns a data time-out event and the transfer is aborted.
The block count register (the MMCHS_BLK[31:16] NBLK bit field) is defined as 16 bits and limits data transfers to a maximum of 65,535 blocks. If the ADMA data transfer size is less than or equal to the 65,535-block transfer, the block count register can be used. In this case, the total length of the descriptor table must be equivalent to "block size" by "block count." If the ADMA data transfer is greater than 65,535 blocks, the block count register must be disabled by setting the block count enable bit ( MMCHS_CMD[1] BCE ) to 0. In this case, the length of the data transfer is not designated by the block count but by the descriptor table.
The timing for detecting the last block on the SD bus may differ, which affects control of the read transfer active (MMCHS_PSTATE[9] RTA), write transfer active (MMCHS_PSTATE[8] WTA), and DAT line active (MMCHS_PSTATE[2] DLA) bits. In case of a read operation, more blocks than required may be read from the card. The host driver must ignore an out-of-range error if the read operation is for the last block of the memory area.