SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
The device supports a suspend feature, which provides a way to stop a closely coupled hardware process running on a peripheral-IP when the host processor enters debug state. The suspend mechanism is important for debug to ensure that peripheral-IPs operate in a lock-step manner with a host controller processor.
An entry is provided for each peripheral-IP that must consider the suspend signals from a number of processors (MPU or DSP). For each peripheral-IP, sensitivity to the suspend signals is defined within two possibilities (and so coded using 1 bit):
For more information about how to program the sensitivity, see the corresponding peripheral-IP TRM chapter.