SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The system direct memory access (DMA_SYSTEM) module, also called DMA4, performs high-performance data transfers between memories and peripheral devices without microprocessor unit (MPU) or digital signal processor (DSP) support during transfer. A DMA transfer is programmed through a logical DMA channel, which allows the transfer to be optimally tailored to the requirements of the application.
The DMA controller includes the following main features:
Figure 18-1 shows an overview of the DMA_SYSTEM module.
Figure 18-1 DMA_SYSTEM OverviewThe DMA_SYSTEM module has three ports: one read, one write, and one configuration port, and provides multiple logical channel support. A dynamically allocated FIFO queue memory pool provides buffering between the read and write ports, which are multithreaded (two threads for the write port and four threads for the read port); this means that each transaction is flagged by a thread ID (0, 1, 2, or 3) in the request direction and in the response direction. This allows the read port to have four outstanding requests at a time. The write port has two threads budget available.
The MPU (or DSP) configures the DMA_SYSTEM through the L4_CFG interconnect.