SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
The BL module arbitrates and merges the memory requests of the ISP master module. The BL module also generates interrupts upon frame completion for the following modules. The interrupt generation is delayed until the transfer completes (acknowledge signal is returned). The following interrupts are delayed by the BL module:
The BL uses two different types of interfaces:
Figure 9-171 show the BL module connections to other submodules of the ISP.
Figure 9-171 ISS ISP BL High-Level Diagram