SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
This event is registered if command list overflow is detected during read or write when software builds a command table with fewer total bytes than the transaction given to the device.
This is a fatal error in which the DMA is in an error state until software clears the SATA_PxCMD[0] ST bit or resets the interface with a port or global reset. For more information about software-initiated resets, see Section 24.8.4.3.2, Software Initiated Resets.