SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
As discussed in the introduction to this chapter, the GPMC module supports the following external memory types:
The following examples describe how to calculate GPMC timing parameters by showing a typical parameter setup for the access to be performed.
The example is based on a 512-Mb multiplexed NOR flash memory with the following characteristics: