SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
In order to facilitate auto-wakeup of DSP C66x, the IDLE protocol’s wakeup capability is used. Wakeup operation is enabled if DSP_SYS_SYSCONFIG[3:2] IDLEMODE is set to 0x3.
In this mode, while in IDLE state, if an external input interrupt source is asserted (if enabled via the DSP_SYS_IRQWAKEEN0 / DSP_SYS_IRQWAKEEN1 mask) or if an external DMA event source is asserted (if enabled via the DSP_SYS_DMAWAKEEN0 / DSP_SYS_DMAWAKEEN1 mask) or if the DSP subsystem NMI input is asserted (note that there is no wake enable mask for the non-maskable interrupt) then the Mwakeup signal is asserted to the PRCM which is expected to observe the Mwakeup. Upon such assertion the PRCM enables the clocks, exiting the "Standby" and "Idle" states. at this point the C66x CPU is able to branch to the pending interrupt service routine. The MWakeup is deasserted when all IRQ or DMA requests enabled in the DSP_SYS_IRQWAKEEN0/1 and DSP_SYS_DMAWAKEEN0/1 are deasserted.
The Wakeup logic controlling assertion of the MWakeup request is completely asynchronous because in IDLE mode the clock may not be present. It relies on level sensitive interrupts.
The DSP_EDMA must be manually removed from IDLE / Standby state. During that time, it is possible that the EDMA input event is no longer pending and may not have been recognized/latched as an EVENT to the EDMA. In that case, the user SW can enable the DSP EDMA_WAKE_INT (in associated DSP_SYS_EDMAWAKE0_IRQENABLE_SET register ) to recognize in the (DSP_SYS_EDMAWAKE0_IRQSTATUS_RAW /DSP_SYS_EDMAWAKE0_IRQSTATUS ) which specific EDMA event was asserted and caused the wakeup condition. The DSP software can then trigger the corresponding DSP_EDMA channel manually (by setting the ESR) or by servicing the interrupt/event manually via reads and writes. For more details, refer to the Section 5.3.5.1.