SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
Many of the Device pads support pad multiplexing. This means that their function can be independently chosen from two or more options. The selection of functions available on each pad is enumerated in the “Multiplexing Characteristics” section of the Data Manual. The desired function is selected via the MUXMODE field of the associated pad configuration register.
By default, the MUXMODE field of most device pads is set to 0xF, which means the pads are in Hi-Z. Only MUXMODE values which correspond to defined functions should be used.
When setting the MUXMODE of any mmc1_* pad, the following register fields should also be programmed: