SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
In the simplest case, the ARP32 branches to the new code section. The existence of program cache provides reasonable performance, especially if the new task program code is cache friendly and is executed a number of times before the next task switch occurs.