SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA75 , DRA750 , DRA752 , DRA756
The Miscellaneous channel type is for any data type that is not a normal video type. The Miscellaneous channel type makes no assumptions on data type and just passes the data to the client and supports a single buffer for the client. The size of the miscellaneous data type is always determined by the Data Type field of the descriptor which specifies the number of bits in the descriptor.
A memory structure used to describe a desired memory transaction to or from a client. The descriptor at a minimum gives an address location for the memory portion of the transfer, the channel to use for this transaction and the size of the transaction. The data descriptor can also contain attributes to be passed down to the client or be linked to another data descriptor to form a larger frame from many smaller frames.