SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
Two-level translation is used when fine-grain granularity is required, that is, when memory sections smaller than 1 MiB are needed. In this case, the first-level descriptor provides a pointer to the base address of a second-level translation table. This second-level table is indexed by bits 19 to 12 of the virtual address. Figure 20-12 shows this indexing mechanism.
Figure 20-12 Two-Level TranslationEach second-level translation table describes the translation of 1 MiB of address space in pages of 64 KiB (large page) or 4 KiB (small page). It consists of 256 second-level descriptors describing 4 KiB each.
In the case of a large page, the same descriptor must be repeated 16 times. If an access points to a descriptor that is not initialized, the MMU will behave in an unpredictable way.