SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA75 , DRA750 , DRA752 , DRA756
The device supports a cross-triggering feature that provides a way to propagate debug (trigger) events from one processor subsystem/module to another. For example, a given subsystem A can be programmed to generate a debug event, which can then be exported as a global trigger across the device. Another subsystem B can be programmed to be sensitive to the trigger line input and to generate an action on trigger detection.
Examples of debug events are: Processor entering debug state, watchpoint match, CS_PTM trigger, and so forth.
Examples of debug actions are: Debug request generation, restart (Cortex-A15 synchronous run), interrupt request generation, start/stop trace, and so forth.
The device implements two global cross-triggering lines: Trigger0 and Trigger1, also referred to as EMU0 and EMU1, respectively.
Subsystem cross-triggering is consolidated at the device level by the XTRIG module, which is embedded in the debug subsystem.
XTRIG is not programmatically visible from the JTAG interface or any device processor. Thus, cross-triggering is programmed at the subsystem level.
The Trigger0 and Trigger1 lines can also be configured as external triggers and contribute to cross-triggering.