SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
Figure 24-200 shows the architecture of the CPTS module inside the GMAC_SW Ethernet Subsystem. Time stamp values for every packet transmitted or received on either port of the GMAC_SW are recorded. At the same time, each packet is decoded to determine if it is a valid time sync event. If so, an event is loaded into the Event FIFO for processing containing the recorded time stamp value when the packet was transmitted or received.
In addition, both hardware (HWx_TS_PUSH) and software (TS_PUSH) can be used to read the current time stamp value though the Event FIFO
Figure 24-200 CPTS Block DiagramThe reference clock used for the time stamp (CPTS_RFT_CLK) can be derived from several sources. See PRCM for more details.