SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA75 , DRA750 , DRA752 , DRA756
The SATA host controller handles data interactions between a local host system memory and a SATA mass storage device with minimal local host (LH) intervention.
In contrast to the parallel 16-bit - ATA (PATA) interface, the SATA interface takes advantage of serial data transmission/reception over a differential pair of conductors. SATA uses the command set from the ATA/ATAPI-6 standard augmented with native command queuing (NCQ) commands optimized for the serialized interface.
The device has one embedded SATA host bus adapter (HBA) controller with a single port. The device SATA host subsystem is composed of several functional components (see Figure 24-151):
For details regarding the device SATA host subsystem components - SATA_PHY , PLLCTRL_SATA, DPLL_SATA and interface adapter), see Section 26.1.1, SATA PHY Subsystem Overview, in Chapter 26, Shared PHY Component Subsystems.
Figure 24-151 shows an overview of the device-embedded SATA host controller subsystem.
Figure 24-151 SATA Host Controller Subsystem Overview