SPRUI30H November 2015 – May 2024
The operation field specifies a limit, save or a jump operation. All of these operations involve two arguments that are specified within the instruction.
In case of limit operation, one of the arguments is a condition and the other argument is a limit register. In case of save operation, one of the arguments is source data and the other argument is a destination where the data will be saved. In jump operation, the first argument is a condition that must be true for the jump to occur and the second argument is a destination to which the program control will be moved to. The destination argument in a jump operation also specifies specific destinations that lead to the current packet being immediately rejected or accepted.
The location of operation field in an instruction is shown in Table 24-909.
| Bits | Description |
|---|---|
| 17:9 | Limit/Save/Jump Operation (operation 0) For limit operation, [17:16] is the operation field, [15:13] is the condition field and [12:9] is a limit register. For save operation, [17:16] is the operation field, [15:13] is the source field, and [12:9] is the destination field. For jump operation, [17:16] is the operation field, [15:13] is the condition field, and [12:9] is the destination field |
| 8:0 | Limit/Save/Jump Operation (operation 1) For limit operation, [8:7] is the operation field, [6:4] is the condition field and [3:0] is a limit register. For save operation, [8:7] is the operation field, [6:4] is the source field, and [3:0] is the destination field. For jump operation, [8:7] is the operation field, [6:4] is the condition field, and [3:0] is the destination field. |
| Description | In a limit operation, the condition argument specifies a condition that must be true for the specified limit register to be decremented if non-zero or the packet to be dropped if the limit register is zero. | ||
| 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | Condition Code | Limit Register | |||||
| Bits | Field Name | Description |
|---|---|---|
| 6:4 | Condition Code | It is a 3-bit code that specifies the condition that must be true for the operation to be executed. 0x0: Single bit flag (flag0 from function 0) 0x1: Single bit flag (flag1 from function 1) 0x2: Logical OR of flags (flag0 | flag1) 0x3: Logical NOR of flags (!(flag0 | flag1)) 0x4: Logical AND of flags (flag0 & flag1) 0x5: Logical NAND of flags (!(flag0 & flag1)) 0x6: XOR of flags (flag0 ^ flag1) 0x7: Unconditional Decrement/Limit |
| 3:0 | Limit Register | It is a 4-bit code that specifies the limit register that is to be decremented or checked for zero value. 0x0: Rate limit register L0 0x1: Rate limit register L1 0x2: Rate limit register L2 0x3: Rate limit register L3 0x4-0xF: Reserved |
| Description | The arguments for a save operation include a code for source data and a code for the destination. The source is either a single bit data or a 32-bit word. The single bit data is either a flag from the functions or a logical OR/AND of the flags. The 32-bit word is the result of the ALU arithmetic/logical functions. | ||
| 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 1 | Source Data Code | Destination Register Code | |||||
| Bits | Field Name | Description |
|---|---|---|
| 6:4 | Source Data Code | It is a 3-bit code that specifies the source data which is to be save in another register 0x0: Single bit flag (flag0 from function 0) 0x1: Single bit flag (flag1 from function 1) 0x2: Logical OR of flags (flag0 | flag1) 0x3: Logical AND of flags (flag0 & flag1) 0x4: Output of function (word0) 0x5: Output of function (word1) 0x6-0x7: Reserved |
| 3:0 | Destination Register Code | It is a 4-bit code that specified the register in which source data is to be stored 0x0-0x3: Single Bit register (T0-T3) 0x4-0x7: Base Register (B1-B3) 0x8-0xF: 32-bit Register (R0-R7) |
For some instructions, the rule engine extracts the operand from the current packet. To determine the packet bits to be used as operands, it refers to one or more base registers. Whenever an instruction causes a change in value of any of the base registers, it cause the rule engine to wait for one clock cycle before executing the next instruction. The rule engine is a pipelined processor and change in the value of a base register causes the prefetched operand values to become stale and these need to be fetched again. The clock cycle inserted allows rule-engine to fetch the data again before the instruction using this data is executed. Only the instructions that use packet data will be delayed by a clock cycle if the previous instruction caused a change in the base register that is referenced in the current instruction.
| Description | For jump operation, one of the operands is a condition that must evaluate to true for the jump operation to occur. The other operand is the destination to which the program counter will move to if the jump operation is executed. The condition in a jump operation is either one of the flags from the output of the arithmetic/logic unit or a logical AND/OR of the flags. | ||
| 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 1 | 0 | Condition Code | Destination Code | |||||
| Bits | Field Name | Description |
|---|---|---|
| 6:4 | Condition Code | Condition Code 0x0: Single bit flag (flag0 from function 0) 0x1: Single bit flag (flag1 from function 1) 0x2: Logical OR of flags (flag0 | flag1) 0x3: Logical NOR of flags (!(flag0 | flag1)) 0x4: Logical AND of flags (flag0 & flag1) 0x5: Logical NAND of flags (!(flag0 & flag1)) 0x6: XOR of flags (flag0 ^ flag1) 0x7: Unconditional Jump |
| 3:0 | Destination Code | Destination Code 0x0: Accept packet, return to instruction zero and wait for the next packet. 0x1: Reject packet and return to instruction zero. 0x2-0xF: Go to instruction at offset +2 ...+15 |
The jump operation results in a change of program execution flow. The jump destination determines the next instruction that will be executed by the rule engine. The destination is only specified as a positive offset to the current value of the program counter. The program counter can result in the rule engine skipping a given number of instructions instead of executing the next instruction. In addition, the destination field can instruct the rule engine to immediately reject or accept the current packet without any further checks. The rule engine then goes back to the first instruction and waits for a new packet to arrive before it executes any further instructions.
The rule engine is a pipelined processor. When it executes a jump operation, there is a delay of one clock cycle before the next instruction is executed.
The operations specified in the two operation fields are independent of each other. However, it is possible that conflicting operations are specified in the operation fields of an instruction. When conflicting operations are specified and conditions of both operations evaluate to true; then the execution flow is determined as described below:
| Description | If there is no Save, Jump or Limit operation specified in the operation field, it is interpreted as a no operation. There is no change in execution flow, no change in any register values or rate limit registers when a no operation is encountered. | ||
| 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 1 | 1 | Reserved | Reserved | |||||
It is expected that the rule engine will be programmed such that a decision to accept or discard the current packet is made before all instructions have executed. If the rule engine reaches the last instruction and it does not result in a decision to accept/reject the packet, then the execution flow does not stop and all instructions from the first instruction are executed again until the end of packet is reached.