SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
This chapter describes the power, reset, and clock management in the device.
For a detailed visual representation of the distribution and management of the device clocks at the PRCM level, see the clock device interactive software for the device CLOCKTREETOOL-AUTOMOTIVE.
Figure 3-1 Clock Tree Tool (CTT)The Clock Tree Tool (CTT) is a Java™-based, stand-alone application. The CTT is interactive clock tree configuration software for the device. The CTT lets the user:
The advantage of the CTT is that the user can visualize the clock tree state of the device on power-on reset and then customize the configuration of the clock tree for the specific use case and identify the device register settings associated to that configuration. Furthermore, the user can dump and read in register settings for the specific scenarios.
Being an interactive visual tool, the CTT gives the user a global view of the device clock tree architecture and allows determining the exact register settings to obtain the specific configuration.