SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
When a resource is owned by the debugger, the resource is released if the debugger is disconnected. Debugger disconnection is accomplished by asserting PIDCON = 0.
If a resource is owned by the application and the processor enters the debug state, the resource continues to belong to the application. The SMSET is not sensitive to debug state.
If SMSET ownership is released while there are still data in the SMSET FIFO, the master port continues to export data to the STM until the FIFO is drained.