SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA75 , DRA750 , DRA752 , DRA756
In the best case (and the most frequent case), the ARP32 CPU takes an interrupt as soon as (very next cycle) it is signaled at its boundary via the cpu_int[15-4]_i or cpu_nmi_i input ports. In this case, the ARP32 CPU takes as little as 5 cycles (from the cycle when the IFR bit gets set) to start executing the first instruction of the ISR:
Note that the ARP32 CPU saves off all architectural registers and other required CPU registers while taking the interrupt (in cycle 1) and as a result the ISR routine does not need to have any instructions to save off the machine state. The ISR routine directly starts executing code related to actual actions to be taken to service the interrupt.