SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
The individual 32-bit counters in the SCTM can be chained with an adjacent counter to form a 64-bit counter. Counters chained to a counter across an even-odd index boundary with the even counter contain the least-significant 32 bits of the 64-bit pairing. For example, counters 1 and 0 can be paired and counter 1 will contain bits 63:32 and counter 0 will contain bits 31:0. The high-order counter increments by 1 each time the low-order counter wraps.
Counters are chained by setting the CACHE_SCTM_CTCR_WT_i[2] CHAIN or CACHE_SCTM_CTCR_WOT_j[2] CHAIN bit for both counters. When chained, the counter control for both counters is taken from the CACHE_SCTM_CTCR_WT_i or CACHE_SCTM_CTCR_WOT_j register of the low-order counter. Other than the CHAIN bit, all other bits in the high-order CACHE_SCTM_CTCR_WT_i or CACHE_SCTM_CTCR_WOT_j register are ignored.
Chained counters can function only in counter mode. Timer mode is not supported.
The CACHE_SCTM_CTCR_WT_i[7] CHNSDW and CACHE_SCTM_CTCR_WOT_j[7] CHNSDW bits are used to indicate that a counter can provide atomics accessed when chained. These bits are valid only for counters with even indexes (the lower half of a 64-bit counter pair). When these bits are set, the counter can shadow the value of the lower half of the chained counter value at the same time the upper half of the counter is read. The shadowed value (not the current value) is returned when the value of the low-order counter is read. Therefore, when a chained counter has atomic read capability, an atomic counter value can be obtained simply by reading the high-order counter first, followed by the low-order counter. This order must always be observed to prevent reading stale counter values from the low-order counter. When counters are functioning independently, the shadow feature is deactivated and a read of the counter always returns the current value.