SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
EVE supports parity-based error detection for all internal data memories (including DMEM, WBUF, IBUFLA, IBUFLB, IBUFHA, and IBUFHB) on the minimum access size granularity of 8 bits (that is, there is 1 bit of parity per byte of memory). EVE subsystem also implements double bit error detection for program cache SRAM through a distance 3, 10-bit Hamming code. The 10-bit Hamming code is also applied to the tag and address for a particular cache line.
When parity is enabled, write accesses to any memory cause the parity/encoding bit(s) to be calculated for the specific write data (along with tag and address value for program cache) and written to the corresponding encoding location. For all read accesses from any data memory, the parity bit is read and compared against previously calculated parity for the current pattern in the memory. For program cache, only ARP32 program fetches perform stored versus expected encoding comparison (accesses through program cache OCP debug target port do not result in code calculation). If a mismatch occurs the error details are recorded in parity error MMR (different for each memory - IBUF, WBUF, DMEM) and the associated interrupt is asserted. At the same time, an OCP error response is generated.
The registers that capture program cache-related parity errors, ARP32 DMEM-related parity errors, WBUF-related parity errors, and IBUF-related parity errors are:
Data returned to the requestor is not modified even in the case of error. The requestor consumes the data potentially causing execution or propagation of bad code and/or data. For a description of the recovery mechanism, see Section 8.1.3.3.6.4, Parity Error Recovery.
Each MMR captures the first occurrence of an error. Software then services the error and clears the MMR to capture subsequent errors (generation of OCP error responses continue if additional errors are detected). The parity error MMRs include bit fields to describe which initiator generated the memory access and the specific byte address. Debug accesses do not cause the error or interrupt registers to be set, but result in OCP error response.
Error interrupts are routed to both ARP32 and as EVE outputs to the device level host. ARP32 services interrupts caused by VCOP, EDMA, or OCP target accesses. However, for errors caused by ARP32 accesses, the ARP32 core is unable to service interrupt, and either the DSP or device local CPU detects and services those errors. This detect and service action is described in Section 8.1.3.10.1, EVE Interrupt Sources – Memory Switch and Parity Error Interrrupts.