SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
RX_PULSE and TX_PULSE interrupts can be paced. The RX_THRESH_PULSE and MISC_PULSE interrupts are not paced. The Interrupt pacing feature limits the number of interrupts that occur during a given period of time. For heavily loaded systems in which interrupts can occur at a very high rate (for example, 148,800 packets per second for Ethernet), the performance benefit is significant due to minimizing the overhead associated with servicing each interrupt. Interrupt pacing increases the processor cache hit ratio by minimizing the number of times that large interrupt service routines are moved to and from the processor instruction cache.
Each RX_PULSE and TX_PULSE interrupt contains an interrupt pacing sub-block (six total). Each sub-block is disabled by default allowing the selected interrupt inputs to pass through unaffected. The interrupt pacing module counts the number of interrupts that occur over a 1 ms interval of time. At the end of each 1 ms interval, the current number of interrupts is compared with a target number of interrupts (specified by the associated maximum number of interrupts register). Based on the results of the comparison, the length of time during which interrupts are blocked is dynamically adjusted. The 1 ms interval is derived from a 4 µs pulse that is created from a prescale counter whose value is set in the INT_PRESCALE field in the WR_INT_CONTROL register. The INT_PRESCALE value should be written with the number of ICLK periods in 4 µs. The pacing timer determines the interval during which interrupts are blocked and decrements every 4 µs. It is reloaded each time a zero count is reached. The value loaded into the pacing timer is calculated by hardware every 1 ms according to the following algorithm:
if (intr_count > 2*intr_max)
pace_timer = 255;
else if (intr_count > 1.5*intr_max)
pace_timer = last_pace_timer*2 + 1;
else if (intr_count > 1.0*intr_max)
pace_timer = last_pace_timer + 1;
else if (intr_count > 0.5*intr_max)
pace_timer = last_pace_timer - 1;
else if (intr_count != 0)
pace_timer = last_pace_timer/2;
else
pace_timer = 0;If the rate of interrupt inputs is much less than the target interrupt rate specified in the associated maximum interrupts register, then the interrupt is not blocked. If the interrupt rate is greater than the target rate, the interrupt will be "paced" at the rate specified in the interrupt maximum register. The WR_C0_RX_IMAX/WR_C0_TX_IMAX register should be written with a value between 2 and 63 inclusive, indicating the target number of interrupts per millisecond.