SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA752 , DRA756
Many systems require the use of a pair of external FIFOs that must be serviced at the same rate. One FIFO buffers data input, and the other buffers data output. The EDMA channels that service these FIFOs can be set up for AB-synchronized transfers. While each FIFO is serviced with a different set of parameters, both can be signaled from a single event.
For example, an external interrupt pin can be tied to the status flags of one of the FIFOs. When this event arrives, the EDMA needs to perform servicing for both the input and output streams. Without the intermediate transfer complete chaining feature this would require two events, and thus two external interrupt pins. The intermediate transfer complete chaining feature allows the use of a single external event (for example, a GPIO event). Figure 16-50 shows the EDMA setup and illustration for this example.
A GPIO event (in this case, GPINT0) triggers an array transfer. Upon completion of each intermediate array transfer of channel 48, intermediate transfer complete chaining sets the E8 bit (specified by TCC of 8) in the chained event register EDMA_TPCC_CER and provides a synchronization event to channel 8. Upon completion of the last array transfer of channel 48, transfer complete chaining—not intermediate transfer complete chaining—sets the E8 bit in EDMA_TPCC_CER (specified by EDMA_TPCC_OPT_n[11] TCCMODE: TCC) and provides a synchronization event to channel 8. The completion of channel 8 sets the I8 bit (specified by EDMA_TPCC_OPT_n[11] TCCMODE: TCC) in the interrupt pending register EDMA_TPCC_IPR, which can generate an interrupt to the CPU, if the I8 bit in the interrupt enable register EDMA_TPCC_IER is set.
Figure 16-50 shows the Intermediate Transfer Completion Chaining Example.
Figure 16-50 Intermediate Transfer Completion Chaining Example