SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
If the internal transmit shift register of the CAN module is ready for loading, and if a data transfer is not occurring between the CAN interface registers and message RAM, the valid message object with the highest priority that has a pending transmission request is loaded into the transmit shift register by the message handler and the transmission is started. The message object's NEWDAT bit in the CANNWDAn register is cleared. After a successful transmission, and if no new data was written to the message object since the start of the transmission, the TXRQST bit in the CANTXRQn register is cleared. If the CAN controller is configured to interrupt on a successful transmission of a message object, (the TXIE bit in the CAN IFn Message Control (CANIFnMCTL) register is set), the INTPND bit in the CANIFnMCTL register is set after a successful transmission. If the CAN module has lost the arbitration or if an error occurred during the transmission, the message is retransmitted as soon as the CAN bus is free again. If, meanwhile, the transmission of a message with higher priority has been requested, the messages are transmitted in the order of their priority.