| 31 |
TS7 |
R/W |
0x0 |
8th Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the eighth sample of the sample sequence.
0x1 = The temperature sensor is read during the eighth sample of the sample sequence.
|
| 30 |
IE7 |
R/W |
0x0 |
8th Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the eighth sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 29 |
END7 |
R/W |
0x0 |
8th Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The eighth sample is the last sample of the sequence.
|
| 28 |
D7 |
R/W |
0x0 |
8th Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS7 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 27 |
TS6 |
R/W |
0x0 |
7th Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the seventh sample of the sample sequence.
0x1 = The temperature sensor is read during the seventh sample of the sample sequence.
|
| 26 |
IE6 |
R/W |
0x0 |
7th Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the seventh sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 25 |
END6 |
R/W |
0x0 |
7th Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The seventh sample is the last sample of the sequence.
|
| 24 |
D6 |
R/W |
0x0 |
7th Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS6 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 23 |
TS5 |
R/W |
0x0 |
6th Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the sixth sample of the sample sequence.
0x1 = The temperature sensor is read during the sixth sample of the sample sequence.
|
| 22 |
IE5 |
R/W |
0x0 |
6th Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the sixth sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 21 |
END5 |
R/W |
0x0 |
6th Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The sixth sample is the last sample of the sequence.
|
| 20 |
D5 |
R/W |
0x0 |
6th Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS5 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 19 |
TS4 |
R/W |
0x0 |
5th Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the fifth sample of the sample sequence.
0x1 = The temperature sensor is read during the fifth sample of the sample sequence.
|
| 18 |
IE4 |
R/W |
0x0 |
5th Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the fifth sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 17 |
END4 |
R/W |
0x0 |
5th Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The fifth sample is the last sample of the sequence.
|
| 16 |
D4 |
R/W |
0x0 |
5th Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS4 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 15 |
TS3 |
R/W |
0x0 |
4th Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the fourth sample of the sample sequence.
0x1 = The temperature sensor is read during the fourth sample of the sample sequence.
|
| 14 |
IE3 |
R/W |
0x0 |
4th Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the fourth sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 13 |
END3 |
R/W |
0x0 |
4th Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The fourth sample is the last sample of the sequence.
|
| 12 |
D3 |
R/W |
0x0 |
4th Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS3 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 11 |
TS2 |
R/W |
0x0 |
3rd Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the third sample of the sample sequence.
0x1 = The temperature sensor is read during the third sample of the sample sequence.
|
| 10 |
IE2 |
R/W |
0x0 |
3rd Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the third sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 9 |
END2 |
R/W |
0x0 |
3rd Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The third sample is the last sample of the sequence.
|
| 8 |
D2 |
R/W |
0x0 |
3rd Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS2 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 7 |
TS1 |
R/W |
0x0 |
2nd Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the second sample of the sample sequence.
0x1 = The temperature sensor is read during the second sample of the sample sequence.
|
| 6 |
IE1 |
R/W |
0x0 |
2nd Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the second sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 5 |
END1 |
R/W |
0x0 |
2nd Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The second sample is the last sample of the sequence.
|
| 4 |
D1 |
R/W |
0x0 |
2nd Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS1 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|
| 3 |
TS0 |
R/W |
0x0 |
1st Sample Temp Sensor Select.
0x0 = The input pin specified by the ADCSSMUXn register is read during the first sample of the sample sequence.
0x1 = The temperature sensor is read during the first sample of the sample sequence.
|
| 2 |
IE0 |
R/W |
0x0 |
1st Sample Interrupt Enable.
It is legal to have multiple samples within a sequence generate interrupts.
0x0 = The raw interrupt is not asserted to the interrupt controller.
0x1 = The raw interrupt signal (INR0 bit) is asserted at the end of the first sample's conversion. If the MASK0 bit in the ADCIM register is set, the interrupt is promoted to the interrupt controller.
|
| 1 |
END0 |
R/W |
0x0 |
1st Sample is End of Sequence.
It is possible to end the sequence on any sample position.
Software must set an ENDn bit somewhere within the sequence.
Samples defined after the sample containing a set ENDn bit are not requested for conversion even though the fields may be non-zero.
0x0 = Another sample in the sequence is the final sample.
0x1 = The first sample is the last sample of the sequence.
|
| 0 |
D0 |
R/W |
0x0 |
1st Sample Differential Input Select.
Because the temperature sensor does not have a differential option, this bit must not be set when the TS0 bit is set.
0x0 = The analog inputs are not differentially sampled.
0x1 = The analog input is differentially sampled. The corresponding ADCSSMUXn nibble must be set to the pair number "i", where the paired inputs are "2i and 2i+1".
|