SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
EPI Read Address 0 (EPIRADDR0), offset 0x024
EPI Read Address 1 (EPIRADDR1), offset 0x034
This register holds the current address value. When performing non-blocking reads via the EPIRPSTDn registers, this register's value forms the address (when used by the mode). That is, when an EPIRPSTDn register is written with a non-0 value, this register is used as the first address. After each read, it is incremented by the size specified by the corresponding EPIRSIZEn register. Thus at the end of a read, this register contains the next address for the next read. For example, if the last read was 0x20, and the size is word, then the register contains 0x24. When a non-blocking read is cancelled, this register contains the next address that would have been read had it not been cancelled. For example, if reading by bytes and 0x103 had been read but not 0x104, this register contains 0x104. In this manner, the system can determine the number of values in the NBRFIFO to drain.
Note that changing this register while a read is active has an unpredictable effect due to race condition.
EPIRADDRn is shown in Figure 16-41 and described in Table 16-25.
Return to Summary Table.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADDR | |||||||||||||||||||||||||||||||
| R/W-0x0 | |||||||||||||||||||||||||||||||