SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
Ethernet MAC Raw Interrupt Status (EMACRIS)
This register identifies the events in the MAC that can generate interrupt.
EMACRIS is shown in Figure 15-29 and described in Table 15-38.
Return to Summary Table.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0x0 | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0x0 | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | LPI | TS | RESERVED | ||||
| R-0x0 | R-0x0 | R-0x0 | R-0x0 | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | MMCTX | MMCRX | MMC | PMT | RESERVED | ||
| R-0x0 | R-0x0 | R-0x0 | R-0x0 | R-0x0 | R-0x0 | ||