SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Higher precision results can be generated using the hardware averaging circuit, however, the improved results are at the cost of throughput. Up to 64 samples can be accumulated and averaged to form a single data entry in the sequencer FIFO. Throughput is decreased proportionally to the number of samples in the averaging calculation. For example, if the averaging circuit is configured to average 16 samples, the throughput is decreased by a factor of 16.
By default the averaging circuit is off, and all data from the converter passes through to the sequencer FIFO. The averaging hardware is controlled by the ADC Sample Averaging Control (ADCSAC) register (see Section 10.5.12). A single averaging circuit has been implemented, thus all input channels receive the same amount of averaging whether they are single-ended or differential.
Figure 10-6 shows an example in which the ADCSAC register is set to 0x2 for 4x hardware oversampling and the IE1 bit is set for the sample sequence, resulting in an interrupt after the second averaged value is stored in the FIFO.
Figure 10-6 Sample Averaging Example