SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Figure 9-3 shows the CBC feedback mode of operation, where the input data is XORed with the IV before it is passed to the basic cryptographic core. The output of the cryptographic core passes directly to the output buffer and becomes the next IV.
The operation is reversed for decryption, resulting in an XOR at the output of the cryptographic core. The input cipher text of the current operation is the IV for the next operation.
Figure 9-3 AES – CBC Feedback Mode