SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
The RTC counting rate can be adjusted to compensate for inaccuracies in the clock source by using the predivider trim register, HIBRTCT. This register has a nominal value of 0x7FFF, and is used for one second out of every 64 seconds in RTC counter mode, when bits [5:0] in the HIBRTCC register change from 0x00 to 0x01, to divide the input clock. Trim is applied every 60 seconds in calendar mode. This configuration allows the software to make fine corrections to the clock rate by adjusting the predivider trim register up or down from 0x7FFF. The predivider trim should be adjusted up from 0x7FFF in order to slow down the RTC rate and down from 0x7FFF in order to speed up the RTC rate.
Care must be taken when using trim values that are near to the subseconds match value in the HIBRTCSS register. It is possible when using trim values above 0x7FFF to receive two match interrupts for the same counter value. In addition, it is possible when using trim values below 0x7FFF to miss a match interrupt.
In the case of a trim value above 0x7FFF, when the RTCSSC value in the HIBRTCSS register reaches 0x7FFF, the RTCC value increments from 0x0 to 0x1 while the RTCSSC value is decreased by the trim amount. The RTCSSC value is counted up again to 0x7FFF before rolling over to 0x0 to begin counting up again. If the match value is within this range, the match interrupt is triggered twice. For example, as shown in Figure 6-5, if the match interrupt was configured with RTCM0 = 0x1 and RTCSSM = 0x7FFD, two interrupts would be triggered.
Figure 6-5 Counter Behavior with a TRIM Value of 0x8002 In the case of a trim value below 0x7FFF, the RTCSSC value is advanced from 0x7FFF to the trim value while the RTCC value is incremented from 0x0 to 0x1. If the match value is within that range, the match interrupt is not triggered. For example, as shown in Figure 6-6, if the match interrupt was configured with RTCM0 = 0x1 and RTCSSM = 0x2, an interrupt would never be triggered.
Figure 6-6 Counter Behavior with a TRIM Value of 0x7FFC